Home > Newsroom > All news > STMicroelectronics’ new GaN ICs platform for motion control boosts appliance energy ratings

STMicroelectronics’ new GaN ICs platform for motion control boosts appliance energy ratings

  • High-efficiency GaN power integrated technology tailored for motor drives in white goods and factory automation
article image

Media Relations

Alexis Breton
Corporate External Communications
Tel: +33.6.59.16.79.08
alexis.breton@st.com

Investor Relations

Jérôme Ramel
EVP Corporate Development & Integrated External Communication
Tel: +41.22.929.59.20
jerome.ramel@st.com

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, has unveiled new smart power components that let home appliances and industrial drives leverage the latest GaN (gallium-nitride) technology to boost energy efficiency, increase performance, and save cost.

 

GaN power adapters and chargers available in the market can handle enough power for laptops and USB-C fast charging to achieve extremely high efficiency to meet stringent incoming eco-design norms. ST’s latest GaN ICs now make this technology applicable to motor drives for products like washing machines, hairdryers, power tools, and factory automation.

 

“Our new GaNSPIN system-in-package platform unleashes wide-bandgap efficiency gains in motion-control applications by introducing special features that optimize system performance and safeguard reliability,” said Domenico Arrigo, General Manager, Application Specific Products Division, STMicroelectronics. “The new devices enable future generations of appliances to achieve higher rotational speed for improved performance, with smaller and lower-cost control modules, lightweight form factors, and improved energy ratings.”

 

The first members of ST’s new family, the GANSPIN611 and GANSPIN612, can power motors of up to 400 Watts including domestic and industrial compressors, pumps, fans, and servo drives. Pin compatibility between the two devices ensures designs are easily scalable. GANSPIN611 is in production now, in a 9mm x 9mm thermally enhanced QFN package, from $4.44.

 

Visitors to SPS – Smart Production Solutions 2025, 25-27 November, at the Nuremberg Exhibition Center, can see the GaNSPIN motor controllers at ST’s booth, no. 271 in Hall 4.

 

Technical notes on GaNSPIN drivers:

 

In the new GaNSPIN system-in-package, unlike in general-purpose GaN drivers, the driver controls turn-on and turn-off times in hard switching to relieve stress on the motor windings and minimize electromagnetic noise. The nominal slew rate (dV/dt) of 10V/ns preserves reliability and eases compliance with electromagnetic compatibility (EMC) regulations such as the EU EMC directive. Designers can adjust the turn-on dV/dt of both GaN drivers to fine-tune the switching performance according to the motor characteristics.

 

With RDS(on) of just 138mΩ in the GANSPIN611 and 270mΩ in the GANSPIN612, the GaN transistors minimize power dissipation and associated self-heating. This lets power components operate without a heatsink in many applications, thereby reducing the bill of materials, while also reducing circuit footprint by up to 60% to permit a smaller, lower-cost PCB.

 

Further features include:

 

• System-in-package with driver and half-bridge power stage with latest-generation 650V GaN power transistors for driving 3-phase BLDC motors

• Integrated bootstrap diode for high-side circuitry

• Suitable for universal 110V – 230V AC offline-powered appliances

• Fault-sensing comparator for smart shutdown provides fast-acting overcurrent protection with programmable disable time

• Undervoltage lockout (UVLO), overvoltage, overcurrent, thermal, and interlocking protection

• Wide supply and input-voltage range up to 20V, for robust and easy conversion of traditional power stages

• Standby pin for power saving

 

About STMicroelectronics

At ST, we are 50,000 creators and makers of semiconductor technologies mastering the semiconductor supply chain with state-of-the-art manufacturing facilities. An integrated device manufacturer, we work with more than 200,000 customers and thousands of partners to design and build products, solutions, and ecosystems that address their challenges and opportunities, and the need to support a more sustainable world. Our technologies enable smarter mobility, more efficient power and energy management, and the wide-scale deployment of cloud-connected autonomous things. We are on track to be carbon neutral in all direct and indirect emissions (scopes 1 and 2), product transportation, business travel, and employee commuting emissions (our scope 3 focus), and to achieve our 100% renewable electricity sourcing goal by the end of 2027. Further information can be found at www.st.com.

Language Versions

Downloads

related-content

Media Relations

Alexis Breton
Corporate External Communications
Tel: +33.6.59.16.79.08
alexis.breton@st.com

Investor Relations

Jérôme Ramel
EVP Corporate Development & Integrated External Communication
Tel: +41.22.929.59.20
jerome.ramel@st.com

Change language Downloads related-content