Home > Newsroom > All news > STMicroelectronics Reveals BlueNRG-2N Network Processor Combining Convenience and Scalability, with Bluetooth® 5.0 Features and Security

Language Versions

STMicroelectronics Reveals BlueNRG-2N Network Processor Combining Convenience and Scalability, with Bluetooth® 5.0 Features and Security

STMicroelectronics has unveiled the BlueNRG-2N Bluetooth 5.0-certified network processor, lowering power consumption and adding support for the latest Bluetooth features that increase data throughput and enhance privacy and security.

The BlueNRG-2N network coprocessor comes pre-programmed, ready for connecting to a host controller to provide Bluetooth connectivity. Not only simplifying product manufacture, the co-processor allows scaling the performance, features, and cost of the host system independently. Designers of products such as smart medical wearables, PC peripherals, remote controls, lighting, industrial and home automation can thus optimize their choice of microcontroller (MCU) to meet specific model requirements.

The latest Bluetooth enhancements featured in BlueNRG-2N include support for Data Length Extension, which accelerates over-the-air (OTA) firmware updates by as much as 2.5 times and raises data transfers to 700kbit/s at the application level. In addition, with support for Bluetooth LE Privacy 1.2, BlueNRG-2N changes address frequently without host-processor involvement to prevent unwanted tracking with minimal impact on system power consumption.

BlueNRG-2N is programmed with a digitally signed Bluetooth LE stack, which saves manufacturing costs while still allowing the flexibility to upgrade OTA. Built-in image authentication technology enhances cyber-security by always checking the stack before starting to allow only signed firmware images to run.

Power consumption is lower compared with previous BlueNRG generations, with low transmit and receive current and drawing just 900nA in shutdown mode with the BLE stack running. At the same time, the device maintains robust and reliable radio performance, with +8dBm programmable RF output power and up to a 96dB link budget.

BlueNRG-2N is the latest member in ST’s BlueNRG family of Bluetooth Low Energy chips that cater to various approaches when designing wireless systems. It shares key features with the BlueNRG-2 Bluetooth 5.0-certified System-on-Chip (SoC), which also contains a programmable Arm® Cortex®-M0 MCU to host the main application and Bluetooth connectivity on the same device. Developers working with BlueNRG chips can take advantage of the powerful and user-friendly STM32* online development environment (ODE), which includes the STM32CubeMX GUI plugin, to kick-start their projects.

As the dedicated network co-processor within the BlueNRG family, BlueNRG-2N is in full production and is included in ST’s 10-year industrial product-longevity program. Devices are available in a 2.66mm x 2.56mm WLCSP34 chip-scale packages: BlueNRG-234N or 5mm x 5mm QFN32: BlueNRG-232N, from $1.21 for orders of 1000 pieces.

Please visit https://www.st.com/bluenrg-2n-pr for more information.

You can also read our blogpost at https://blog.st.com/bluenrg-2n/

* STM32 is a registered and/or unregistered trademark of STMicroelectronics International NV or its affiliates in the EU and/or elsewhere. In particular, STM32 is registered in the US Patent and Trademark Office.

Language Versions

Change language