Home > Newsroom > All news > STMicroelectronics to showcase Edge AI and automation solutions at SEMICON Southeast Asia 2025

Language Versions

STMicroelectronics to showcase Edge AI and automation solutions at SEMICON Southeast Asia 2025

  • More than 10 exciting demos addressing Edge AI and sensors, wireless connectivity, automotive, and factory-automation solutions
  • ST will be speaking on Advanced Packaging, Sustainability, MEMS for Medical Applications, and Talent Acquisition

Media Relations

Dennis Tan
STMicroelectronics

Dennis Tan
STMicroelectronics
Tel: +65 6216 5000
wddennis.tan@st.com

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, is exhibiting at SEMICON Southeast Asia 2025 (Booth L1901) on May 20-22.

 

The booth will feature more than 10 exciting demos including Edge AI & Sensors with gesture recognition, Wireless Connectivity solutions for personal electronics and home appliances, Automotive solutions for battery monitoring and charging co-developed with EDOM, and a robotic-automation demo developed with OMRON to showcase automation in the cleanroom.

 

Edge AI & Sensors
AI Assistant: This demo is an intelligent personal assistant terminal enhanced by various AI features implemented in the STM32N6 microcontroller (MCU). The AI assistant works with a pose estimation demo powered by YOLOv8n, showcasing its ability to understand and respond to human gestures, and the inference time could reach 25 fps.

 

Robotic Hand demo: This demo shows a system that utilizes the STM32N6 MCU to run a gesture recognition model through the N6’s built-in neural processing unit (NPU), coupled with the VD66GY high-sensitivity color image sensor, to achieve gesture recognition. The STM32MP257 PLC demonstration board then converts the data format of the 21 identified key point data, allowing the motion of the 15 servo motors in the dexterous hand to be controlled for real-time gesture tracking.

 

Smart Presence/Gesture Control: The demo detects human presence and reacts to hand control behavior to wake-up and respond-to instructions. It is powered by the VL53L8CX 8×8 multizone, ToF ranging sensor, which enhances performance under ambient-light conditions with reduced power consumption.

 

ST ISPU with Sliding Discrete Fourier Transform: The ISPU (Intelligent Sensor Processing Unit) is ST’s latest edge-computing core. DSP code developed by the application can be ported into the ISPU and runs in an IMU (Inertial Measurement Unit). FT (Fourier Transform) is one of the essential functions for condition monitoring in today’s AI enabled Industrial applications. SDFT (Sliding Discrete Fourier Transform) is loaded into this AI core to demonstrate the capability of the ISPU.​

 

Biosensors: An accelerometer embeds a vAFE (vertical analog front-end) and an AI core with Machine Learning and Finite State Machine. It is able to detect biopotentials by means of the external electrodes connected to the device to provide the data for ENG, ECG, EEG, Heart-Rate and Motion-Detection applications.​

 

Wireless Connectivity Solutions
ST60 Wireless Data Transfer: The ST60A2 is an RF millimeter-wave transceiver operating in the 60 GHz VBand. It provides a very power-efficient and high data-rate wireless link enabling freedom from physical cables and connectors for short-range (a few cm) point-to-point communications, using a variety of external antennas (such as patch antennas designed on a PCB or highly directive SMT horn antennas allowing both end-fire and broadside radiation patterns).

 

Ki Cordless Kitchen: The demo showcases the newly designed ST Ki power transmitter combined with ST’s NFC devices. Ki Cordless Kitchen is a new standard developed by the Wireless Power Consortium (WPC), to replace power cords in traditional kitchen appliances (e.g., mixer, toaster, rice cooker, coffee maker) and integrate them with induction cooktops. The ST power transmitter is combined with both “static” and “dynamic” appliances to demonstrate different modes and power control. It uses ST’s IH-series IGBTs for efficient power management and an STM32G4 MCU for precise control and seamless operation. While ST’s integrated NFC technology enables effortless connectivity, a secure cooking environment is ensured by STSAFE technology to safeguard user data.

 

Automotive solutions
The e-2 wheeler demo has been built by ST and EDOM, an esteemed distribution partner of ST. The demo showcases 4 key solutions including battery-management system, smart compact battery charger, energy-efficient traction inverter, and an NFC keyless system solution.

 

OMRON robot demonstration
Leveraging Industry 4.0 to advance manufacturing capabilities, ST deployed robotic solutions in its manufacturing facility in Ang Mo Kio, Singapore to automate wafer cassette handling, previously a strenuous manual process. These robots now operate 22 different machines efficiently 24/7, leading to a productivity gain of 10%. This also freed up additional resources among workers, who were then trained in higher-value skillsets benign to their career progression. Through a structured Career Development Plan (CDP), operators and technicians are advancing to higher technical roles, with over 100 employees benefiting from this initiative.

Onsite robotics experience
ST will be organizing hands-on robotics sessions onsite on May 22, targeting 12-18 year olds. The aim is to engage and interest them in STEM and robotics applications in their formative years. These workshops are conducted in small-sized groups for greater engagement and effectiveness. Limited seats are available and interested parties can apply here: https://stmicroelectronics.eightfold.ai/events/candidate/landing?plannedEventId=xKnvZ1RkpG

 

Speaking slots
As part of its thought-leadership and knowledge sharing, ST will also be engaged in several speaking opportunities throughout the event addressing topics of Advanced Packaging, Sustainability, MEMS for Medical Applications, and also on Talent Acquisition. For more details on specific onsite forums/summits, please visit https://www.semiconsea.org/

 

 Advanced Packaging & Heterogeneous Integration Summit
Speaker: David Gani, Director, Back-end Manufacturing and Technology R&D
Topic: Panel Level Packaging: Challenges and advantages in packaging R&D and high-volume production
Date: 21 May
Time: 10:00 – 17:00hrs
Note: Paid entry

 

Sustainability Forum
Speaker: Edoardo Auteri, Head of Sustainability Programs – Asia Pacific excluding China Region
Topic: Accelerating sustainable transformation in technology and beyond to reduce emissions
Date: 22 May
Time: 09:30 – 13:30hrs
Note: Paid entry

 

Smart MedTech Forum
Speaker: Alberto Leotti, MEMS R&D, Lab-in-Fab Operations Manager
Topic: A new wave of sensors for vital sign monitoring
Date: 22 May
Time: 10:00 – 15:00hrs

Note: Paid entry

Workforce Development Stage
Speaker: Choon Fatt Chong
Topic: STMicroelectronics: Our Technology starts with You
Date: 22 May
Time: 12.40pm
Note: Complimentary entry

 

About STMicroelectronics
At ST, we are 50,000 creators and makers of semiconductor technologies mastering the semiconductor supply chain with state-of-the-art manufacturing facilities. An integrated device manufacturer, we work with more than 200,000 customers and thousands of partners to design and build products, solutions, and ecosystems that address their challenges and opportunities, and the need to support a more sustainable world. Our technologies enable smarter mobility, more efficient power and energy management, and the wide-scale deployment of cloud-connected autonomous things. We are on track to be carbon neutral in all direct and indirect emissions (scopes 1 and 2), product transportation, business travel, and employee commuting emissions (our scope 3 focus), and to achieve our 100% renewable electricity sourcing goal by the end of 2027. Further information can be found at www.st.com.

Language Versions

Media Relations

Dennis Tan
STMicroelectronics

Dennis Tan
STMicroelectronics
Tel: +65 6216 5000
wddennis.tan@st.com

Change language