Home > Newsroom > All news > "Technology Starts with You": The first-ever ST Taiwan Tech Day focuses on four mega trends to showcase the latest innovations

Language Versions

"Technology Starts with You": The first-ever ST Taiwan Tech Day focuses on four mega trends to showcase the latest innovations

article image

Media Relations

Vicky Ho
STMicroelectronics
Tel: +886 2 6603 2505
vicky.ho@st.com

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, is holding its first-ever ST Taiwan Tech Day at the Taipei New Horizon on November 2. The event is designed to provide valued customers and partners with the most up-to-date information on ST products and solutions to facilitate innovation and achieve success.

 

With the theme “Our Technology Starts with You,” this extensive technology event will offer insightful speeches and showcase over 40 demonstrations centered around four mega trends: Smart Mobility, Power & Energy, IoT & Connectivity, and Sensing the World. Attendees can experience first-hand the latest innovations and learn how ST’s technologies are contributing to a safer, greener, and more connected world. It will also be a great opportunity to help developers and innovators stay ahead of the curve in today’s rapidly evolving market.

 

Innovation highlights

 

Smart Mobility
Zonal Gateway: Zonal Gateway acts as a bridge between the automotive central computer and traditional signal-based ECUs. This technology is supported by ST’s wide range of automotive-grade products and enables Service-Oriented Architecture (SOA) with Data Distribution Service (DDS) protocol and Firmware Over-The-Air (FOTA). The Zonal Gateway offers a solution for modernizing automotive systems, allowing for seamless communication between different components and enabling efficient and secure updates.

 

3rd-Generation SiC Modules: The industry leader in Silicon Carbide (SiC), ST offers a wide range of solutions to help developers improve the power efficiency and reduce the size and weight of automotive inverters with its 3rd-generation SiC modules. The traction inverter is a critical component in electric vehicles as it converts energy from the battery to drive the motors in the drivetrain. These converters must handle high power and currents, provide fail-safe operation, and handle EMC challenges. Alongside the SiC modules, ST’s range of solutions includes AEC-Q101 qualified IGBTs, silicon and silicon-carbide MOSFETs and diodes, AEC-Q100 qualified galvanically isolated IGBT and MOSFET gate drivers, and SPC5 32-bit automotive microcontrollers. These offerings enable scalable, cost-effective, and energy-efficient EV traction inverter solutions.

 

Power & Energy
Digital Power: ST’s digital power solution is a comprehensive set of reference designs that empower designers to create efficient, feature-rich power supplies for a wide range of applications. The demo highlights two powerful solutions: the 25kW DAB DC/DC converter with ST’s ACEPACK module, a highly efficient and reliable power converter ideal for industrial and automotive applications, and the 30kW Gen3 SiC MOSFET three-phase interleaved LLC solution with an STM32G4 MCU for ultra-high voltage EV charger — a cutting-edge power supply designed to provide ultra-fast charging for electric vehicles.

With these solutions, designers can create custom power systems that are efficient, reliable, and tailored to their specific needs.

 

Precision Position Control: ST is a leading technology provider for motor control and servo drives, offering power device technologies, computational processing, isolated devices, industrial safety, ecosystem for industrial automation, connectivity, and predictive maintenance. With ST’s state-of-the-art motor-control technologies, the motor can precisely control movement to a specific position. The demo consists of two small BLDC motors that can hold two shapes that do not fit together when they are in phase. The precision motor-control algorithm enables the rotation and movement of the shapes towards each other at any time, offsetting the relative position of the two shapes by 90 degrees while rotating. This unique position allows coupling between the shapes, with a rotation speed that ensures the phase shift is not noticeable, demonstrating precision position control in a harmonic movement coordinated simultaneously with other shapes.

 

IoT & Connectivity
Edge AI Washing Machine Solution: This solution utilizes artificial intelligence (AI) to achieve unparalleled levels of energy and water efficiency by accurately measuring the weight of clothes inside the machine. The AI model generated by ST’s NanoEdge AI Studio significantly improves measurement accuracy compared to traditional algorithms by analyzing and learning the features of current signals. This technology can advance the washing-machine industry to a next level by optimizing energy and water consumption while providing more accurate measurements.

 

Compact Production Line with IO-Link System: The IO-Link automated product line demonstrates ST’s total solution application in a smart factory, utilizing IO-Link technology to manage digital input/output, sensors, and solenoid air valve drivers. The demos include digital IO boards, sensor boards, and actuator boards from ST’s Automation Competence Center’s reference demo boards. The IO-Link products simplify the installation, setup, maintenance, and repair of factory automation systems, enhancing system flexibility to produce different product models. The IO-Link diagnostic function enables smarter and more reliable factory operations.

 

Sensing the World
3D Sensing Solutions: ST showcases the advanced imaging capabilities of the 3D stereo-vision camera solutions for machine-vision applications. The eYs3D stereo camera reference design features ST’s high-performance, near-infrared VD56G3 global-shutter image sensors, ensuring the highest quality depth sensing and point-cloud creation. Additionally, the VD55H1 low-noise, low-power, indirect Time-of-Flight (iToF) sensor die, manufactured using advanced backside-illuminated, stacked-wafer technology, enables the creation of a small form-factor 3D camera capable of producing high-definition depth maps with a typical ranging distance of up to 5 meters in full resolution and beyond 5 meters with patterned illumination. This demo highlights ST’s commitment to providing cutting-edge technology for machine-vision applications.

 

ISPU for personal electronics: ISPU (Intelligent Sensor Processing Unit) is a new processing category embedded in ST’s LSM6DSO16IS MEMS module. It is an ultra-low-power, high-performance programmable core that can execute signal processing and AI algorithms in real-time. The ISPU offers C programming and an enhanced ecosystem with libraries and 3rd-party tools/IDE, making it a state-of-the-art feature for any personal electronics.

 

In addition to the insightful speeches and exciting technology showcase, more than 20 in-depth technical presentations covering Smart Mobility, Power and Energy, and IoT and Connectivity will provide a close look at the cutting-edge technologies that are shaping our world.

 

To learn more about the exciting demos and program, please visit the ST Taiwan Tech Day event page.

 

About STMicroelectronics
At ST, we are over 50,000 creators and makers of semiconductor technologies mastering the semiconductor supply chain with state-of-the-art manufacturing facilities. An integrated device manufacturer, we work with more than 200,000 customers and thousands of partners to design and build products, solutions, and ecosystems that address their challenges and opportunities, and the need to support a more sustainable world. Our technologies enable smarter mobility, more efficient power and energy management, and the wide-scale deployment of the Internet of Things and connectivity. We are committed to achieving our goal to become carbon neutral on scope 1 and 2 and partially scope 3 by 2027. Further information can be found at www.st.com.

Language Versions

Media Relations

Vicky Ho
STMicroelectronics
Tel: +886 2 6603 2505
vicky.ho@st.com

Change language