Home > Newsroom > All news > STMicroelectronics introduces first STM32-ready wireless IoT modules leveraging collaboration with Qualcomm

Language Versions

Downloads

related-content

STMicroelectronics introduces first STM32-ready wireless IoT modules leveraging collaboration with Qualcomm

WiFi6/Bluetooth 5.3/Thread ST67W611M1 modules accelerate development and boosts flexibility to deliver advanced consumer and industrial IoT solutions

article image

Media Relations

Alexis Breton
Corporate External Communications
Tel: +33.6.59.16.79.08
alexis.breton@st.com

Investor Relations

Jérôme Ramel
EVP Corporate Development & Integrated External Communication
Tel: +41.22.929.59.20
jerome.ramel@st.com

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, has introduced the first product of its strategic collaboration with Qualcomm Technologies to simplify development of next-generation wireless solutions for industrial and consumer IoT applications. The collaboration aims to deliver initially IoT modules leveraging ST’s powerful STM32 ecosystem and Qualcomm Technologies’ leading wireless connectivity solutions.

 

The first of these modules, the ST67W611M1, contains a Qualcomm® QCC743 multiprotocol connectivity system-on-a-chip (SoC), pre-loaded with Wi-Fi6, Bluetooth 5.3 qualified, and Thread combo, made easy to integrate with any STM32 microcontroller (MCU) or microprocessor (MPU). The module will support Matter protocol over Wi-Fi for future-proof connectivity, making the STM32 portfolio seamlessly accessible to the Matter ecosystem. Aiding the system integration, the module also contains 4Mbyte Flash for code and data storage, and a 40MHz crystal. There is also an integrated PCB antenna or micro RF (uFL) connector for an external antenna.

 

“Our collaboration delivers multiple advantages for the large community that leverage the STM32 family in their embedded systems,” said Remi El-Ouazzane, President, Microcontrollers, Digital ICs and RF Products Group (MDRF) at STMicroelectronics. “Qualcomm’s expertise in highly influential and widely used wireless connectivity technologies is now at product developers’ fingertips and combines with the powerful software, tools, features and project acceleration offered by the STM32 development ecosystem.”

 

“This is just the beginning of our mission, which we expect to deliver many further successes enabling new and advanced edge processing applications,” said Rahul Patel, Group General Manager, Connectivity, Broadband and Networking Business Unit, Qualcomm Technologies, Inc. “We look forward to continuing our collaboration with STMicroelectronics to bring more unparalleled connected experiences with Wi-Fi, Bluetooth, AI, 5G and more.”

 

Advanced hardware security is built in, with hardware cryptographic accelerators, as well as services including secure boot and secure debug, reaching PSA Certified Level 1 protection. The module is self-contained and pre-certified according to mandatory specifications, requiring no RF design expertise from the user to create a working solution. Highly integrated in a 32-lead LGA package, it is ready to place on the board and permits simple, low-cost PCB designs with as few as two layers.

 

The ST67W611M1 leverages the STM32 ecosystem, which contains over 4,000 commercial part numbers, powerful STM32Cube tools and software, and enhancements that boost edge AI development. AI enhancements include the recently introduced STM32N6 MCUs, which contain ST’s Neural-ART Accelerator, and the ST Edge AI Suite that provides an AI Model Zoo and STM32Cube.AI and NanoEdge AI optimization tools.

 

The modules are designed to be quickly and seamlessly integrated with any STM32 microcontroller or STM32 microprocessor, which offer flexible options for performance, price, and power across a broad spectrum. The MCUs available range from cost- and power-sensitive devices containing the Arm® Cortex®-M0+ core to devices containing high performing cores such as Cortex-M4 and Cortex-A7 in the STM32MP1/2 MPUs.

 

Samples of the ST67W611M1 are available, with OEM availability in Q1 2025, with broader availability in Q2 2025. To request samples and pricing options please contact your local ST sales office.

 

For more information, please go to www.st.com/st67w

 

You can also refer to the press release of October 2024: STMicroelectronics and Qualcomm enter strategic collaboration in wireless IoT

 

STM32 is a registered and/or unregistered trademark of STMicroelectronics International NV or its affiliates in the EU and/or elsewhere. In particular, STM32 is registered in the US Patent and Trademark Office.

Qualcomm and Snapdragon products mentioned within this press release are offered by Qualcomm Technologies, Inc. and/or its subsidiaries. Qualcomm and Snapdragon are trademarks or registered trademarks of Qualcomm Incorporated.

 

About STMicroelectronics
At ST, we are over 50,000 creators and makers of semiconductor technologies mastering the semiconductor supply chain with state-of-the-art manufacturing facilities. An integrated device manufacturer, we work with more than 200,000 customers and thousands of partners to design and build products, solutions, and ecosystems that address their challenges and opportunities, and the need to support a more sustainable world. Our technologies enable smarter mobility, more efficient power and energy management, and the wide-scale deployment of cloud-connected autonomous things. We are committed to achieving our goal to become carbon neutral on scope 1 and 2 and partially scope 3 by 2027. Further information can be found at www.st.com.

Language Versions

Downloads

related-content

Media Relations

Alexis Breton
Corporate External Communications
Tel: +33.6.59.16.79.08
alexis.breton@st.com

Investor Relations

Jérôme Ramel
EVP Corporate Development & Integrated External Communication
Tel: +41.22.929.59.20
jerome.ramel@st.com

Change language Downloads related-content