Home > Newsroom > All news > STMicroelectronics Accelerates Innovation in Automotive Electronics with Powerful Development Tools

Language Versions

STMicroelectronics Accelerates Innovation in Automotive Electronics with Powerful Development Tools

  • AutoDevKit™ ecosystem simplifies prototyping state-of-the-art automotive Electronic Control Units
  • Easily connects robust SPC5 microcontrollers with boards with automotive devices
  • Free to download, easy to use, application-programming software and source code provided

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, is helping the automotive industry deliver safer, greener, and smarter vehicles to market more quickly and cost effectively with new tools that assist the development of electronic control units (ECUs), the ‘mini-computers’ that manage the numerous electronic systems in today’s vehicles.

The automotive market is changing quickly, transitioning from familiar technologies such as ordinary bulbs, mechanical systems, and hydraulics to lightweight, intelligent replacements such as LEDs and brushless motors, amid the general trend toward electrification and digitalization. New vehicles can contain over 100 ECUs and, as their complexity is always increasing, design teams need to accelerate development to keep pace.

ST’s AutoDevKit™ ecosystem introduces a new and efficient toolset for creating working prototypes, replacing traditional artisan approaches and supporting standardization and design reuse. Available for free, the AutoDevKitlibrary is a software environment that lets users select the microcontrollers and functional boards from ST’s wide automotive portfolio to easily prototype an automotive solution.

After choosing the preferred AutoDevKit components, users are guided to connect the boards, generate code, compile and download firmware, without forgetting prototype testing and debugging. A fundamental aspect of the AutoDevKit ecosystem is to offer easy-to-use application-program interfaces (API) for communication and control for each of the functional boards supported.

“Automotive-electronics designers are under intense time-to-market pressure and delivering a credible proof of concept quickly is critical,” said Marco Monti, President, Automotive and Discrete Group, STMicroelectronics. “Our AutoDevKit ecosystem can cut months of engineering effort from traditional prototype development by letting users concentrate on system functionality and offload low-level tasks such as building device drivers.”
The AutoDevKit software is part of the integrated design environment for ST’s SPC5 automotive microcontrollers.

ST will demonstrate AutoDevKit technology at Embedded World 2020, Hall 4A Stand 138. Readers can visit www.st.com/autodevkit-ew2020 and register to receive an AutoDevKit board free of charge during the show.

Further technical information
The complete AutoDevKit ecosystem includes the AutoDevKit library plugin and hardware development tools including AEK MCU discovery and functional boards and AEKD System Solution Demonstrators that are optimized for automotive use.
The AEK tools include discovery boards for evaluating specific automotive microcontrollers and functional boards that help quickly implement various functions such as motor control, LED lighting, power management, audio, and connectivity. Dedicated APIs are available for each board to control the features and facilitate communication, all without having a deep knowledge of the semiconductor devices employed or their datasheets.
The AEKD System Solution Demonstrators provide direct access to pre-assembled system-demonstrator boards, as well as board kits and non-electronic hardware assemblies such as car-like components and loads to help users closely emulate the desired solution.
AutoDevKit is fully integrated with SPC5 Studio software development environment and extends the IDE functionalities with automatic pin allocation for the microcontroller and board view editor dedicated to support users to interconnect several functional boards with the microcontroller board. Similarly, AutoDevKit APIs are fully integrated with SPC5 Studio low-level drivers delivering code that is readily portable across microcontroller platforms.
Further information and free downloads at http://www.st.com/autodevkit

About STMicroelectronics
ST is a global semiconductor leader delivering intelligent and energy-efficient products and solutions that power the electronics at the heart of everyday life. ST’s products are found everywhere today, and together with our customers, we are enabling smarter driving and smarter factories, cities and homes, along with the next generation of mobile and Internet of Things devices.
By getting more from technology to get more from life, ST stands for life.augmented.
In 2019, the Company’s net revenues were $9.56 billion, serving more than 100,000 customers worldwide. Further information can be found at www.st.com.

For Press Information Contact:
Michael Markowitz
Director Technical Media Relations
STMicroelectronics

Tel: +1 781 591 0354
Email: michael.markowitz@st.com

Language Versions

Change language