Home > Newsroom > All news > New demonstration board from STMicroelectronics kickstarts dual-motor designs for advanced industrial and consumer products

New demonstration board from STMicroelectronics kickstarts dual-motor designs for advanced industrial and consumer products

Highly integrated STSPIN32G4 motor controller accelerates time to market leveraging STM32 ecosystem

article image

STMicroelectronics’ EVSPIN32G4-DUAL demonstration board controls two motors from a single STSPIN32G4 integrated driver, accelerating product development and simplifying the PCB design and bill of materials.

 

The EVSPIN32G4-DUAL board cuts the time to market for advanced industrial and consumer products such as robots, multi-axis factory automation systems, garden equipment, and power tools. The STSPIN32G4 motor controller contains an Arm® Cortex®-M4 microcontroller (MCU) with the processing power to manage both motors simultaneously, executing complex algorithms like field-oriented control (FOC) in real-time. In addition, MCU peripherals support sensored or sensorless FOC and advanced position and torque-control algorithms, including motor-control and general-purpose timers, analog functions including operational amplifiers and comparators.

 

The EVSPIN32G4-DUAL demonstration board leverages an advanced three-phase gate driver integrated in the STSPIN32G4 and an additional STDRIVE101 gate driver to control two three-phase inverters delivering up to 10A with a maximum supply voltage of 74V. Both gate drivers have their own bootstrap circuitry and safety features including drain-source voltage monitoring, cross-conduction prevention, several thermal protection mechanisms, and under-voltage lockout (UVLO).

 

EVSPIN32G4-DUAL also leverages the STSPIN32G4’s built-in power-management circuitry, permitting a compact design with a low BOM that is easy to procure and permits rapid assembly in production. The power management includes a programmable buck converter for gate drivers VCC supply, a low-dropout linear regulator, and a special regulator with low quiescent current to supply the MCU during standby.

 

The STSPIN32G4 is included in the STM32 ecosystem that provides extensive support for application development, including tools for starting the project, middleware packs, and software examples. The X-CUBE-MCSDK (motor control software development kit) has firmware libraries for algorithms including FOC and STM32 motor-control workbench. This is an easy-to-use graphical tool that lets the user select and automatically configure the EVSPIN32G4-DUAL directly from a menu.

 

EVSPIN32G4-DUAL is available now from www.st.com and distributors, for $145.

 

For further information please visit www.st.com/evspin32g4-dual

 

STM32 is a registered and/or unregistered trademark of STMicroelectronics International NV or its affiliates in the EU and/or elsewhere. In particular, STM32 is registered in the US Patent and Trademark Office.

Language Versions

Downloads

related-content

Change language Downloads related-content