Home > Newsroom > All news > Updates Add Video to STMicroelectronics’ TouchGFX Suite for Richer STM32 User Experiences

Language Versions


Notice: Trying to access array offset on value of type null in /opt/newsroom.st.com/wp-content/themes/st-news-v2/template-parts/content/content-single-article.php on line 43

Updates Add Video to STMicroelectronics’ TouchGFX Suite for Richer STM32 User Experiences

STMicroelectronics has released TouchGFX Version 4.18 for user-interface development with STM32* microcontrollers (MCUs), adding video playback, enhanced tools for multi-developer collaboration, and support for new X-NUCLEO display kits.

By allowing playback of Motion-JPEG (MJPEG) video files, TouchGFX brings extra pizzazz to small devices like home-automation products, wearables, medical devices, and industrial sensors, allowing rich features such as instructional guides or entertaining startup and pause screens to enhance the user interface. Developers can use their own MJPEG files or choose from the sample movies provided. A new video widget in TouchGFX Designer, with properties including start, stop, repeat, and go-to-frame, simplifies prototyping and is added to the application by drag and drop.

TouchGFX 4.18 allows video decoding in either software or hardware. Hardware decoding is possible with STM32 MCUs that contain a suitable decoding peripheral, such as the STM32F769 and STM32H7B3. Software decoding is available on all series devices except the STM32G0 series. Various strategies for video buffering, including direct rendering to the frame buffer and double buffering, help optimize memory demand and performance.

Additional new features of TouchGFX 4.18 include enhanced support for collaborative working, using XML to store text data and translations. XML simplifies sharing and merging various elements of the project as multiple team members contribute. The powerful and convenient features of previous TouchGFX versions are retained, including the partial frame buffer for very low RAM use, ultra-efficient rendering that prevents tearing effects, and support for low-cost non-memory-mapped SPI Flash.

For an easy start to GUI development projects, TouchGFX 4.18 comes with examples showing how to use the new video capabilities and the necessary TouchGFX Board Setup (TBS) for the popular STM32 Discovery boards.

ST has also updated and extended the selection of display shields that help developers quickly get their user-interface projects running. The updated X-NUCLEO-GFX01M2 for Nucleo 64 boards has a 2.2” QVGA serial interface display and now supports the NUCLEO-WB55RG, making it easy to add a display to a Bluetooth® application. A new X-NUCLEO-GFX02Z1 for Nucleo 144 has a high-speed parallel interface and QSPI Flash memory on-board, supporting among others the NUCLEO-U575ZI-Q Both are supported in TouchGFX 4.18.

TouchGFX 4.18 is available now, free of charge, from st.com. The new X-NUCLEO-GFX02Z1 Nucleo 144 Display Shield is also available now, at a retail price of $35.00. The X-NUCLEO- GFX01M2 will be available in December, also at $35.00.

For further information please go to https://www.st.com/content/st_com/en/ecosystems/stm32-graphic-user-interface.html.

You can also read our blogpost at https://blog.st.com/touchgfx-418/.

* STM32 is a registered trademark of STMicroelectronics International NV or its affiliates in the EU and/or elsewhere. In particular, STM32 is registered in the US Patent and Trademark Office.

Language Versions

Change language
Notice: Trying to access array offset on value of type null in /opt/newsroom.st.com/wp-content/themes/st-news-v2/template-parts/content/content-single-article.php on line 311

Notice: Trying to access array offset on value of type null in /opt/newsroom.st.com/wp-content/themes/st-news-v2/template-parts/content/content-single-article.php on line 324