search-history

Bookmark

Home > Newsroom > All news > STMicroelectronics Releases KNX-RF Software for Power-Conscious Building Automation

Language Versions


Notice: Trying to access array offset on value of type null in /opt/newsroom.st.com/wp-content/themes/st-news-v2/template-parts/content/content-single-article.php on line 43

STMicroelectronics Releases KNX-RF Software for Power-Conscious Building Automation

  • Online demonstrations scheduled for KNXperience (Sep 28-Oct 2)

STMicroelectronics has released KNX software for the S2-LP ultra-low-power radio transceiver to enable energy-saving standardized wireless connectivity for smart-building controls.

Ready to run on an STM32* microcontroller (MCU) or alternatively on a BlueNRG-2 Bluetooth® Low Energy System-on-Chip (SoC) that embeds an Arm® Cortex®-M0 core running at 32MHz and a comprehensive set of I/O peripherals, the software contains a certified KNX-RF stack, RF adaptation layer, and S2-LP library needed to connect the transceiver to create an ultra-low-power wireless KNX node. Operating in the 868.3MHz band at only 10mA with +10dBm output, the S2-LP delivers market-leading energy efficient, secure and robust wireless connectivity prolonging battery run-time and reducing the overall cost of the solution.

Combining the S2-LP radio and BlueNRG-2 SoC enables a unique hybrid and low-power optimized KNX/Bluetooth solution in two chips, allowing a smartphone to access KNX-based networks and provide an intuitive and stylish interface for conveniently monitoring, controlling, configuring, provisioning, and updating the KNX nodes.

Whether hosted on the BlueNRG-2 or STM32 MCU, ST’s KNX-RF software enables innovation and power savings for push-buttons, light switches, occupancy sensors, roller-shutter controls, dimmer actuators, and other devices for lighting, heating, HVAC, and energy-harvesting systems.

The software meets the latest KNX-RF Multi specification, which supports secure (S mode), encrypted communications and frequency agility with five channels to help avoid interference and permit fast and slow communication modes to save power. Further features of KNX-RF Multi boost reliability and allow larger numbers of KNX devices to coexist on the network, including listen before talk (LBT), fast acknowledge with auto-retry, and support for repeaters.

To create the new KNX-RF Multi software, ST teamed with its Authorized Partners, Tapko for the certified KNX stack and Actimage for the RF adaptation layer.

The S2-LP package joins ST’s STKNX highly integrated transceiver for KNX TP communication over twisted-pair cable and extends the Company’s portfolio of certified solutions for smart-building communication, which comprehensively covers the major industry standards. In addition to enabling both wired and wireless KNX specifications with these solutions, ST provides embedded software, evaluation tools, and mobile apps to accelerate the development of Bluetooth Low Energy Mesh and 6LoWPAN networking solutions for smart-building and industrial applications. Both S2-LP and BlueNRG-2 devices belong to the ST 10-year longevity program.

As a Gold Sponsor of the KNXperience online tradeshow running September 28 to October 2, ST will present demonstrations during the event that leverage the KNX RF Multi software package with interoperability using legacy KNX-TP and ETS to configure and control light switches, adjust LED color and dimming, and setup KNX devices with a smartphone connected through the BlueNRG-2 Bluetooth SoC.

Please visit www.st.com/s2-lp-pr for more information.

 

* STM32 is a registered and/or unregistered trademark of STMicroelectronics International NV or its affiliates in the EU and/or elsewhere. In particular, STM32 is registered in the US Patent and Trademark Office.

Language Versions

Change language
Notice: Trying to access array offset on value of type null in /opt/newsroom.st.com/wp-content/themes/st-news-v2/template-parts/content/content-single-article.php on line 311

Notice: Trying to access array offset on value of type null in /opt/newsroom.st.com/wp-content/themes/st-news-v2/template-parts/content/content-single-article.php on line 324