search-history

Bookmark

Home > Newsroom > All news > STMicroelectronics Simplifies IoT-Node Connectivity and Security with Latest STM32 Discovery Kit and Expansion Software

Language Versions


Notice: Trying to access array offset on value of type null in /opt/newsroom.st.com/wp-content/themes/st-news-v2/template-parts/content/content-single-article.php on line 43

STMicroelectronics Simplifies IoT-Node Connectivity and Security with Latest STM32 Discovery Kit and Expansion Software

STMicroelectronics is simplifying the complex software challenges that face developers of IoT nodes by introducing the B-L4S5I-IOT01A STM32 Discovery kit. The kit comes with a qualified port of FreeRTOS™, fully integrated into the STM32Cube ecosystem and ready to connect to Amazon Web Services (AWS).

The hardware comprises an STM32L4+ microcontroller board that contains an extensive selection of ST MEMS sensors, an STSAFE-A110 secure element, Bluetooth® 4.2 and Wi-Fi® modules, and an NFC tag with printed antenna for flexible, low-power communication with cloud servers. Coming with the X-CUBE-AWS v2.0 STM32Cube Expansion Pack, the kit can be used as a reference design to simplify and accelerate completion of the final product.

The X-CUBE-AWS v2.0 pack ensures proper integration of the FreeRTOS standard AWS connectivity framework within the STM32Cube environment. This lets users take advantage of both FreeRTOS and STM32Cube without developing additional software. It also supports AWS native services including standard Firmware Over The Air (FOTA) tasks and handles interactions with the on-board STSAFE-A110 secure element, including taking care of AWS IoT Core Multi-Account Registration and assigning security-critical operations during boot-up, device authentication, and OTA firmware verification.

The STM32L4+ board is featured to meet the performance demands and energy constraints typically placed on IoT nodes. The STM32L4S5VIT6 ultra-low-power Arm® Cortex®-M4 microcontroller combines 2MB Flash, 640KB RAM, digital and analog peripherals, and hardware encryption accelerator. The on-board sensors comprise the HTS221 capacitive digital relative-humidity and temperature sensor, LIS3MDL high-performance 3-axis magnetometer, LSM6DSL 3D accelerometer and 3D gyroscope, LPS22HB absolute digital output barometer, VL53L0X Time-of-Flight and gesture-detection sensor, and two digital omnidirectional microphones.

The B-L4S5I-IOT01A Discovery kit can be ordered directly from www.st.com or distributors for $54.00. The X-CUBE-AWS v2.0 STM32Cube Expansion Pack is ready to download free of charge.

For further information please visit http://www.st.com/b-l4s5i-iot01a.

STM32 is a registered and/or unregistered trademark of STMicroelectronics International NV or its affiliates in the EU and/or elsewhere. In particular, STM32 is registered in the US Patent and Trademark Office.

Language Versions

Change language
Notice: Trying to access array offset on value of type null in /opt/newsroom.st.com/wp-content/themes/st-news-v2/template-parts/content/content-single-article.php on line 311

Notice: Trying to access array offset on value of type null in /opt/newsroom.st.com/wp-content/themes/st-news-v2/template-parts/content/content-single-article.php on line 324