search-history

Bookmark

About Us > Newsroom > All news > STMicroelectronics launches a new advanced 6-axis IMU with embedded sensor fusion and AI

Language Versions

STMicroelectronics launches a new advanced 6-axis IMU with embedded sensor fusion and AI

article image

ST has introduced LSM6DSV16X, the flagship 6-axis inertial measurement unit (IMU) embedding ST’s Sensor Fusion Low Power (SFLP) technology, Artificial Intelligence (AI), and adaptive-self-configuration (ASC) for superior power optimization.
The advanced architecture of the LSM6DSV16X enables sophisticated processing in the edge, making the device ideal for advanced 3D phone mapping, context awareness in laptops and tablets, reliable and precise gesture recognition for XR headsets, as well as always-on activity tracking. All the processing is done in the MEMS sensor itself, which also contains a triple sensing core to meet the differing needs of user-interface controls and optical/electronic image stabilization (OIS/EIS).
The IC integrates an enhanced finite state machine (FSM), to detect fast events and custom gestures. In addition, the latest updates to ST’s innovative machine-learning core (MLC) raise the performance of inference algorithms such as human activity recognition. ST has published ready-to-use MLC and FSM algorithms on GitHub to help product designers cut time to market when implementing these advanced capabilities in new products. The IMU also makes the AI features, extracted by MLC, available for external processing.

With ASC, the sensor can optimize its own settings such as measurement range and operating frequency, independently and on the fly, without host intervention. Teamed with ST’s Sensor Fusion Low Power (SFLP) technology, it enables the IMU to host fast and powerful edge processing with minimal energy demand. SFLP allows gesture recognition or continuous tracking while drawing as little as 15µA.

In addition, LSM6DSV16X integrates for the first time in an IMU a charge-variation (ST Qvar®) sensing channel to monitor changes in electrostatic charge, either through electrodes in contact with the body in a smartwatch or fitness band or by non-contact sensing (“radar”). ST MEMS sensors with ST Qvar® support advanced user-interface controls such as touch, long press, and swipe, which ensure seamless interactions.

As a high-accuracy 6-axis MEMS IMU, the LSM6DSV16X contains a 3-axis low noise accelerometer and 3-axis gyroscope for accurate sensing in an industry-standard size and with the new I3C interface. Both structures benefit from high stability after reflow soldering, which saves equipment manufacturers recalibrating the IMU on the production line and guarantees sensing performance.

The LSM6DSV16X is in production now in a 2.5mm x 3.0mm x 0.83mm 14-lead LGA package, priced from $2.98 for orders of 1000 pieces. ST will continue to expand the Generation 3 lineup by adding more sensors with differing levels of performance and capability in the coming months.

For further information, please visit www.st.com/lsm6dsv16x

Ready-to-use MLC and FSM algorithms are available on GitHub at

https://github.com/STMicroelectronics/STMems_Machine_Learning_Core/tree/master/application_examples/lsm6dsv16x

https://github.com/STMicroelectronics/STMems_Finite_State_Machine/tree/master/application_examples/lsm6dsv16x

Language Versions

Change language